LPC84x where do I find the IAP/ISP driver or API?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC84x where do I find the IAP/ISP driver or API?

2,185件の閲覧回数
jespermadsen
Contributor III

I Installed the MCUXpresso IDE v10.3.0 and made a project with SDK_2.x_LPC844.. 

But it dosen't seem to include any api for ISP?

What is the procedure?

タグ(1)
3 返答(返信)

2,013件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jesper,

You are right MCUXpresso SDK doesn't include IAP driver files.

You can find it in LPCOpen

or

in EEPROM demo code: LPC8xx EEPROM Emulation 

Have a great day,
Jun Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,013件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,013件の閲覧回数
jespermadsen
Contributor III

Thank you Jun Zhang. 

:smileyhappy:

Take care..

0 件の賞賛
返信