LPC84x where do I find the IAP/ISP driver or API?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC84x where do I find the IAP/ISP driver or API?

2,205 Views
jespermadsen
Contributor III

I Installed the MCUXpresso IDE v10.3.0 and made a project with SDK_2.x_LPC844.. 

But it dosen't seem to include any api for ISP?

What is the procedure?

Tags (1)
3 Replies

2,033 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jesper,

You are right MCUXpresso SDK doesn't include IAP driver files.

You can find it in LPCOpen

or

in EEPROM demo code: LPC8xx EEPROM Emulation 

Have a great day,
Jun Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,033 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,033 Views
jespermadsen
Contributor III

Thank you Jun Zhang. 

:smileyhappy:

Take care..

0 Kudos
Reply