LPC845 reinvoke_ISP not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845 reinvoke_ISP not working

1,920 Views
pasqualebarrega
Contributor II

I'm using LPC845 internal bootloader, when I invoke the command "Reinvoke ISP" from flash or from ram I obtain this error: "0x1C     REINVOKE_ISP_CONFIG              Reinvoke ISP not successful"

I have tried to invoke this command also after SystemInit (before starting others application tasks) but nothing changed.

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

1,769 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Pasquale,

Are you using the Code Bundle or the MCUXpresso SDK as base for your application? Which ISP interface are you selecting? If using USART ISP mode, make sure to enable the clocks to the default before calling this command.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply