LPC845,how to use external crystal as the chip clock source?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845,how to use external crystal as the chip clock source?

ソリューションへジャンプ
2,534件の閲覧回数
Roger_WANG_2022
Contributor I

I use the LPC845-Example-Code-Bundle-IAR code to test my board. when I try to use SystemInit() (system.c)to initialize my system clock. some definitions was chip_setup.h. My question is how to config these. For example, I want to use 12M external crystal as clock source, and get 30Mhz.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
2,367件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Roger Wang,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to use the MCUXpresso Config Tools to configure the clock, the tool provides a GUI allows developers to quickly build a custom clock and generate initialization C code for a custom board, so please give a try.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,368件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Roger Wang,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I'd highly recommend you to use the MCUXpresso Config Tools to configure the clock, the tool provides a GUI allows developers to quickly build a custom clock and generate initialization C code for a custom board, so please give a try.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信