LPC845 UART Clock settings for different baudrate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 UART Clock settings for different baudrate

1,989件の閲覧回数
jtro
Contributor III

I'm looking for Clock settings for different UART baudrate. I have tried with different clock but many times it stuck at assert due to wrong clock configuration. 

Even i can't see any % error in peripheral configuration so that clock value can be adjusted.

Also I observed that, if  frg0_clk is select as clock source then I'm not getting correct clock value from CLOCK_GetUart0ClkFreq() .

It would be great if any information on Clock rate settings for different baud rate such as 9600,19200,38400,57600,115200.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,805件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello jtro 9 ,

Could you please tell me which version of Configuration Tool do you used, or you use the MCUXpresso IDE?

Also share your project and the error you mentioned.

Recommend you use the latest config tool and SDK.

BR

Alice

0 件の賞賛
返信