LPC845 SCTimer/PWM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845 SCTimer/PWM

4,758 Views
keyzet_89
Contributor I

Good day.
For the initial setup of the LPC845, I use MCUXpresso Config Tools. I need to configure SCTimer/PWM as PWM in two outputs and multiple events mode (OUT_0 use 2 events, OUT_1 use 4 events). All events is "Match event only". The program throws an error "Number of events exceeds 8 events supported by peripheral SCT0 (each PWM signal internally allocates 2 events)." Is it true? Or can I configure multiple events on one output manually? For example:

const sctimer_pwm_signal_param_t SCTimer_0_pwmSignalsConfig[2] = {
  {
    .output = kSCTIMER_Out_0,
    .level = kSCTIMER_LowTrue,
    .dutyCyclePercent = 0
  },
  {
    .output = kSCTIMER_Out_1,
    .level = kSCTIMER_LowTrue,
    .dutyCyclePercent = 0
  }
};

void SCTimer_0_init(void)
{
  SCTIMER_Init(SCTIMER_0_PERIPHERAL, &SCTimer_0_initConfig);
  // OUT_0, 2 events
  SCTIMER_SetupPwm(SCTIMER_0_PERIPHERAL, &SCTimer_0_pwmSignalsConfig[0], kSCTIMER_EdgeAlignedPwm, DEF_M_FRQ, SCTIMER_0_CLOCK_FREQ, &SCTimer_0_pwmEvent[0]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 6000, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[0]);
  SCTIMER_SetupOutputSetAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_0, SCTimer_0_event[0]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 12000, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[5]);
  SCTIMER_SetupOutputClearAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_0, SCTimer_0_event[5]);
  SCTIMER_IncreaseState(SCTIMER_0_PERIPHERAL);
  // OUT_1, 4 events
  SCTIMER_SetupPwm(SCTIMER_0_PERIPHERAL, &SCTimer_0_pwmSignalsConfig[1], kSCTIMER_EdgeAlignedPwm, DEF_M_FRQ, SCTIMER_0_CLOCK_FREQ, &SCTimer_0_pwmEvent[1]);
  SCTIMER_ScheduleEvent(SCTIMER_0_PERIPHERAL, SCTimer_0_event[0]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 25, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[1]);
  SCTIMER_SetupOutputSetAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_1, SCTimer_0_event[1]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 5975, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[2]);
  SCTIMER_SetupOutputClearAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_1, SCTimer_0_event[2]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 6025, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[3]);
  SCTIMER_SetupOutputSetAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_1, SCTimer_0_event[3]);
  SCTIMER_CreateAndScheduleEvent(SCTIMER_0_PERIPHERAL, kSCTIMER_MatchEventOnly, 11975, kSCTIMER_Out_0, kSCTIMER_Counter_L, &SCTimer_0_event[4]);
  SCTIMER_SetupOutputClearAction(SCTIMER_0_PERIPHERAL, kSCTIMER_Out_1, SCTimer_0_event[4]);
}

Labels (2)
Tags (2)
0 Kudos
Reply
5 Replies

4,420 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Владимир Орлов

Yes, each PWM allocates 2 events, one for the pulse period and the other for the frequency. To set multiple events you can use SCTIMER_CreateAndScheduleEvent() function.

Also I suggest you to take a look to this document SCTimer/PWM cookbook. This contains a collection of examples and usage notes for the SCTimer/PWM block.

 

Let me know if this is helpful.

Best regards,

Omar

4,420 Views
keyzet_89
Contributor I

Good afternoon, Omar.
Thanks for your reply. Yes, this document is very useful. But the question still remained. This document on pages 14-15 has an example of Simple PWM. Can I change it to fit my task in this way?

void SCT_Init(void)
{
    LPC_SCT->CONFIG        |= (1 << 17);                // two 16-bit timers, auto limit
    LPC_SCT->CTRL_L        |= (12-1) << 5;              // set prescaler, SCTimer/PWM clock = 1 MHz
                                               
    LPC_SCT->MATCHREL[0].L  = 10-1;                     // match 0 @ 10/1MHz = 10 usec (100 kHz PWM freq)
    LPC_SCT->MATCHREL[1].L  = 4;                        // match 1 used for duty cycle (in 10 steps)
    LPC_SCT->MATCHREL[2].L  = 6;                        // match 2 used for duty cycle (in 10 steps)
    LPC_SCT->MATCHREL[3].L  = 8;                        // match 3 used for duty cycle (in 10 steps)
 
    LPC_SCT->EVENT[0].STATE = 0xFFFFFFFF;               // event 0 happens in all states
    LPC_SCT->EVENT[0].CTRL  = (1 << 12);                // match 0 condition only
 
    LPC_SCT->EVENT[1].STATE = 0xFFFFFFFF;               // event 1 happens in all states
    LPC_SCT->EVENT[1].CTRL  = (1 << 0) | (1 << 12);     // match 1 condition only
    
    LPC_SCT->EVENT[2].STATE = 0xFFFFFFFF;               // event 1 happens in all states
    LPC_SCT->EVENT[2].CTRL  = (2) | (1 << 12);          // match 1 condition only / event 2 associate with match 2
    
    LPC_SCT->EVENT[3].STATE = 0xFFFFFFFF;               // event 1 happens in all states
    LPC_SCT->EVENT[3].CTRL  = (3) | (1 << 12);          // match 1 condition only / event 3 associate with match 3
 
    LPC_SCT->OUT[0].SET     = (1 << 0) | (1 << 2);                 // event 0 and event 2 will set   SCTx_OUT0
    LPC_SCT->OUT[0].CLR     = (1 << 1) | (1 << 3);                 // event 1 and event 3 will clear SCTx_OUT0
 
    LPC_SCT->CTRL_L        &= ~(1 << 2);                // unhalt it by clearing bit 2 of CTRL reg
}

Will this work as intended?

Best regards, Владимир.

0 Kudos
Reply

4,420 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Владимир Орлов

 

Can you tell me what are intended to do? With the information I have I'm not able to tell you if it works, I would need to put me on your application context.

 

Best regards,

Omar

0 Kudos
Reply

4,420 Views
keyzet_89
Contributor I

Good afternoon, Omar.
In fact, I need to get something like this output signal. Two outputs, the frequency is 2 times different and there is a phase shift. The severity is different. Thus, output_1 is obtained as in the example with Simple PWM. However, output_0 will have 4 events - 2 on SET and 2 on CLR. The total number of events 8 does not exceed. After re-reading the user manual, I did not find in it restrictions on the number of events per output.
Sorry for such a weird schedule. The brown dotted line is the beginning of the counter.

2019-09-19_09-43-25 копия.jpg

Best regards, Владимир.

0 Kudos
Reply

4,420 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello Владимир Орлов.

I agree with you, the number of events needed for your application does not exceed the permitted one. I suggest to check this example as a guide to design your application "max_sctimer_multi_state_pwm". This example can be found at the sdk.

 

On the example focus on the function SCTIMER_SetupPwm(). This function configures the PWM parameters and sets 2 events with SCTIMER_CreateAndScheduleEvent()

Use this function as reference to design your function for the PWM of your OUT_0. Add the events with SCTIMER_CreateAndScheduleEvent()

 

You may find a more detailed explanation of each function at the example driver.

 

Let me know if this is helpful

Best regards,

Omar

0 Kudos
Reply