LPC845 SCTimer PWM issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845 SCTimer PWM issues

4,013 Views
AgustinOrdonez
Contributor I

Hello, im trying to use a PWM, i've read the CookBook so I did the following:

#include "LPC845.h"

void setDuty(uint8_t duty);
int main(){
       //SW, SCTimer,GPIO1,ICON
	SYSCON->SYSAHBCLKCTRL0 |= (1<<7) | (1<<8)|(1<<18)|(1<<20);


	SCT->CONFIG |= (1<<0)|(1<<17);
	SCT->MATCH[0]=FREQ_CLOCK_MCU/1000;
	SCT->MATCHREL[0]=FREQ_CLOCK_MCU/1000;

	SCT->EV[0].STATE=0xFFFFFFFF;
	SCT->EV[0].CTRL= 0 | (1<<12);
	SCT->OUTPUT=0xC;
	SCT->RES=0b01010101;
	SCT->EVEN=1;


	SCT->EV[1].STATE=0xFFFFFFFF;
	SCT->EV[1].CTRL = 1 | (1<<12);
	SCT->OUT[0].SET = 1;
	SCT->OUT[0].CLR = (1<<1);

	SCT->MATCH[1] = 1;
	SCT->MATCHREL[1] = 1;

	NVIC->ISER[0] = (1<<9);

	SWM0->PINASSIGN.PINASSIGN8=1*32+1; //BLUE LED

	SCT->CTRL &= ~(1 << 2);

	setDuty(20);

	while(1){}

    return 0;
}

void setDuty(uint8_t duty){
	SCT->MATCHREL[1] = FREQ_CLOCK_MCU/1000*duty/100;
}

However this doesn't work, i've spent like 5 hours thinking about this and can't find why can anyone help on this? I am not using any SDK on purpose. This does turn on the blue led on the board (I turn off all LEDs first but didn't paste it here)

0 Kudos
Reply
6 Replies

3,983 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For your code, pls refer to the modification.

 

 

#include "LPC845.h"

void setDuty(uint8_t duty);
int main(){
       //SW, SCTimer,GPIO1,ICON
	SYSCON->SYSAHBCLKCTRL0 |= (1<<7) | (1<<8)|(1<<18)|(1<<20);   
        SYSCON->SCTCLKsel=1; //USE MAIN CLOCK AS sct CLOCK
        SYSCON->SCTCLKDIV=1; //enable the SCT clock



	SCT->CONFIG |= (1<<0)|(1<<17);
	SCT->MATCH[0]=FREQ_CLOCK_MCU/1000;
	SCT->MATCHREL[0]=FREQ_CLOCK_MCU/1000;

	SCT->EV[0].STATE=0xFFFFFFFF;
	SCT->EV[0].CTRL= 0 | (1<<12);
	SCT->OUTPUT=0xC;
	SCT->RES=0b01010101;
	SCT->EVEN=1;


	SCT->EV[1].STATE=0xFFFFFFFF;
	SCT->EV[1].CTRL = 1 | (1<<12);
	SCT->OUT[0].SET = 1;
	SCT->OUT[0].CLR = (1<<1);

	SCT->MATCH[1] = FREQ_CLOCK_MCU/(2*1000);
	SCT->MATCHREL[1] = FREQ_CLOCK_MCU/(2*1000);

	NVIC->ISER[0] = (1<<9);

	SWM0->PINASSIGN.PINASSIGN8=1*32+1; //BLUE LED

	SCT->CTRL &= ~(1 << 2);

	setDuty(20);

	while(1){}

    return 0;
}

void setDuty(uint8_t duty){
	SCT->MATCHREL[1] = FREQ_CLOCK_MCU/(1000*2);
}

 

 

Pls try to use the above code.

I suppose that you'd better connect a scope to PIO1_1 and check if the PWM signal appears. You can not see the LED toggles, because the PWM is 1KHz signal, it is too fast to sere the LED toggles, the LED always turns on.

If you have not scope and have to use LED to see PWM, you can output low frequency PWM signal for example 1Hz and check if the LED toggles with the following configuration.

SCT->MATCH[0]=SCT->MATCHREL[0]=FREQ_CLOCK_MCU/1;
SCT->MATCH[1]=SCT->MATCHREL[1]=FREQ_CLOCK_MCU/2;

If you still have issue, pls check the SCT->COUNT in tools debugger and if the counter changes it's value.

Hope it is helpful

BR

XiangJun Rong

0 Kudos
Reply

3,957 Views
AgustinOrdonez
Contributor I

Well, tried what you sent (on 1Hz)and it doesn't flicker. How could I check SCT->COUNT?

0 Kudos
Reply

3,963 Views
AgustinOrdonez
Contributor I

Thanks, i'll try that. I know I can't see the flicker with 1kZ PWM, but with duty at 20% the brightness should be a lot lower, which it isn't.

0 Kudos
Reply

3,938 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I will have a test next week. for the following code, the SCT0 counter can count tick, but the red led can not toggle, I have not a scope on hand, I will test with a scope next week.

BR

XiangJun Rong

#define FREQ_CLOCK_MCU 18000000
void SCTimerInit(void)
{
//SW, SCTimer,GPIO1,ICON
SYSCON->SYSAHBCLKCTRL0 |= (1<<7) | (1<<8)|(1<<18)|(1<<20);
SYSCON->SCTCLKSEL=1; //USE MAIN CLOCK AS sct CLOCK
SYSCON->SCTCLKDIV=1; //enable the SCT clock

 

SCT0->CONFIG |= (1<<0)|(1<<17);
SCT0->MATCH[0]=(uint32_t)(FREQ_CLOCK_MCU/1);
SCT0->MATCHREL[0]=(uint32_t)(FREQ_CLOCK_MCU/1);

SCT0->EV[0].STATE=0xFFFFFFFF;
SCT0->EV[0].CTRL= 0 | (1<<12);
SCT0->OUTPUT=0xC;
SCT0->RES=0b01010101;
SCT0->EVEN=1;


SCT0->EV[1].STATE=0xFFFFFFFF;
SCT0->EV[1].CTRL = 1 | (1<<12);
SCT0->OUT[0].SET = 1<<1;
SCT0->OUT[0].CLR = 1;

SCT0->MATCH[1] = (uint32_t)(FREQ_CLOCK_MCU/(2*1));
SCT0->MATCHREL[1] = (uint32_t)(FREQ_CLOCK_MCU/(2*1));

//NVIC->ISER[0] = (1<<9);

//SWM0->PINASSIGN.PINASSIGN8=1*32+15; //BLUE LED
SWM0->PINASSIGN.PINASSIGN8=0; //P0_0 green led

SCT0->CTRL &= ~(1 << 2);

setDuty(20);

while(1){}

}

0 Kudos
Reply

3,901 Views
AgustinOrdonez
Contributor I

Managed to make it work with the following code:

    SYSCON->SYSAHBCLKCTRL0 |= (1<<7) | (1<<8)| (1<<18) | (1<<20);

	SWM0->PINASSIGN.PINASSIGN7 &= ((32*1+2 << 24) | 0x00FFFFFF);; //RED LED

	SCT->CONFIG |= (1<<0)|(1<<17);
	SCT->MATCH[0]=FREQ_CLOCK_MCU/(1000); //1KHz on unidrectional mode
	SCT->MATCHREL[0]=FREQ_CLOCK_MCU/(1000);

	SCT->EV[0].STATE=1; //any number except 0
	SCT->EV[0].CTRL= 0 | (1<<12);
	SCT->OUTPUT=0xC;
	SCT->RES=0b01010101;
	SCT->EVEN=1;

	SCT->EV[1].STATE=1;//any number except 0
	SCT->EV[1].CTRL = 1 | (1<<12);
	SCT->OUT[0].SET = 1; 
	SCT->OUT[0].CLR = (1<<1);

	SCT->MATCH[1] = 0;
	SCT->MATCHREL[1] = 0;

	SCT->CTRL &= ~(1 << 2);

Removed interruption and changed PINASSIGN on SWM

0 Kudos
Reply

3,922 Views
AgustinOrdonez
Contributor I

Thanks, i'll tell you if I can fix it in the weekend

0 Kudos
Reply