LPC845 PIO0_30 missing

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC845 PIO0_30 missing

跳至解决方案
3,117 次查看
lubomirbogdanov
Contributor II

Hello guys,

If I go to the LPC845 datasheet on page 8, fig. 5, the LQFP48 package has a pin number 42 which corresponds to PIO0_30. If I go to the LPC845 user guide in section 11.5 I/O configuration register description, I cannot find such a pin.

If I go to PIO1_30 in that same document I see a table name:

Table 250. PIO0_30 register (PIO0_30, address 0x4004 40CC) bit description

So which one is true? I'm a bit confused.

Thanks in advance,

L. B.

标签 (1)
0 项奖励
回复
1 解答
3,010 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thanks for your reply.
Actually, the LPC845 series don't have the PIO1_31 pin.

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,010 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
In section 11.5 I/O configuration register description of LPC845's user guide, the Table 199 contains the PIO0_30 actually.

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
3,010 次查看
lubomirbogdanov
Contributor II

OK, I see!

Can we say that the register PIO1_30 has the same structure of the bit fields as PIO0_30?

0 项奖励
回复
3,011 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thanks for your reply.
Actually, the LPC845 series don't have the PIO1_31 pin.

pastedImage_1.png

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复