LPC845 Example Code Bundle MCUXpresso issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845 Example Code Bundle MCUXpresso issue

3,454 Views
NeoTsai
Contributor II

Hi support team,

   I have download LPC845 example code from web.

import the projects to MCUXpresso IDE.

it has some project settings are wrong.

something like

PROJECT_LOC/../../Source_Code/GPIO_PatternMatch/docs

have to change to 

PROJECT_LOC/docs

0 Kudos
Reply
2 Replies

1,874 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Neo,

Please make sure that while importing the examples projects to your workspace the "Copy projects into workspace" option is selected:

pastedImage_1.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos
Reply

1,874 Views
NeoTsai
Contributor II

Hi Carlos,

   yes, I have copy the projects to my workspace.

i think there is something different with OS. 

Or the file path is not correct.

I am using macOS.

The file Path is as follow shows.

sh-3.2# cd LPC845workspace/

sh-3.2# ls

.DS_Store I2C_Wakeup_Slave

.metadata Multi_Timer_Blinky

ADC_Seqa_Seqb PMU_Modes

Analog_Comparator ROM_Divide

CapTouch_3Sensor_Slider SCT_Event_Counter

CapTouch_6Sensor_Wheel SCT_Event_Timer

CapTouch_9Sensor_Button SCT_PWM_2State

CapTouch_Wakeup_9Sensor_Button SPI0M_SPI1S

Ctimer_PWM SPI_Wakeup_Master

DAC SPI_Wakeup_Slave

DMA_UART UART0_Terminal

DeepPD_WKT USART1M_USART2S

FAIM_and_Clocks USART_Wakeup_Master

Flash_IAP USART_Wakeup_Slave

GPIO_Interrupts WWDT

GPIO_PatternMatch common

I2C_MasterSlave peripherals_lib

I2C_Wakeup_Master utilities_lib

sh-3.2# cd common

sh-3.2# ls

.DS_Store README_MCUXpresso_Projects.txt

.cproject inc

.project

sh-3.2# cd inc

sh-3.2# pwd

/User/NeoTsai/Documents/MCUXpressoIDE_10.1.0/LPC845workspace/common/inc

sh-3.2#

0 Kudos
Reply