LPC845 DAC1 Configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC845 DAC1 Configuration

跳至解决方案
2,412 次查看
kk7xo
Contributor III

I am using the LPCXpresso845-MAX board and wish to use DAC1 which is connected to the speaker.  In the schematic for the board it shows that the speaker is connected to DAC1 via pin PIO0_29. 

Referring to the LPC845 user manual UM11029 rev 1.7 of April 2021 I see that in the IOCON register for DAC0, PIO0_17, there is a DACMODE bit (number 16) that must be set to use DAC0, but in IOCON register for PIO0_29 there is no corresponding bit for DAC1. 

How do I set DACMODE for DAC1 in PIO0_29?

 

0 项奖励
回复
1 解答
2,400 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kk7xo 

There isn't this bit, no need config DACMODE bit.

 

BR

Alice

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,401 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @kk7xo 

There isn't this bit, no need config DACMODE bit.

 

BR

Alice

0 项奖励
回复
2,386 次查看
kk7xo
Contributor III
Thank you!
0 项奖励
回复