LPC845 BRK schematic - missing pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 BRK schematic - missing pin

ソリューションへジャンプ
2,031件の閲覧回数
lubomirbogdanov
Contributor II

Hello, guys!

By looking at the circuit diagram of LPC845 BRK RevA breakout board I cannot tell where does the PIO1_7 go? Is it connected to CN1 at all?

I need to do a pin toggle exactly on this pin to test my firmware for a custom PCB that uses LPC845.

Regards,

Lubo

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
1,928件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,929件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信