LPC845 BRK schematic - missing pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC845 BRK schematic - missing pin

Jump to solution
2,106 Views
lubomirbogdanov
Contributor II

Hello, guys!

By looking at the circuit diagram of LPC845 BRK RevA breakout board I cannot tell where does the PIO1_7 go? Is it connected to CN1 at all?

I need to do a pin toggle exactly on this pin to test my firmware for a custom PCB that uses LPC845.

Regards,

Lubo

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
2,003 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,004 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply