LPC845 BRK schematic - missing pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC845 BRK schematic - missing pin

跳至解决方案
2,119 次查看
lubomirbogdanov
Contributor II

Hello, guys!

By looking at the circuit diagram of LPC845 BRK RevA breakout board I cannot tell where does the PIO1_7 go? Is it connected to CN1 at all?

I need to do a pin toggle exactly on this pin to test my firmware for a custom PCB that uses LPC845.

Regards,

Lubo

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,016 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,017 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Lubomir Bogdanov,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is the PIO1_7 pin connected to CN1 at all?
-- No, this pin is floated.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复