LPC845 ADC Hardware Trigger (CTIMER0_MAT3)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC845 ADC Hardware Trigger (CTIMER0_MAT3)

1,595件の閲覧回数
riteshpanchal00
Contributor I

Hello,

I am using LPCXpresso845MAX kit.

I want to Verify Amplitude and Frequency of 60Hz Sine Wave through ADC.

I am planning to Use ADC with CTIMER0_MAT3 Hardware Trigger (Match 3 channel of CTIMER0).

I have configured ADC channel 3 in Sequence B and other ADC channel (which are software triggered used for other purpose) in Sequence A.

ADC.png

And configured CTIMER with 0.16ms timer interval. (100 ADC sample for 60Hz(=16.66ms) period)

Ctimer.png

But I am not getting ADC Sequence B Interrrupt.

0 件の賞賛
返信
1 返信

1,569件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Ritesh Panchal ,

Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
I'd like to suggest you'd better go through the generated code firstly, maybe you can find something miss.
In addition, the post (DMA Ping-Pong application ) presents how to use the SCTimer to trigger the ADC to start a conversion sequence, it may give you some insight.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信