LPC844 examples for Keil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC844 examples for Keil

2,906 Views
KoComputes
Contributor II

Hi all, I'ld appreciate some advice to become productive with the LPC844 in Keil MDK.

The project uses I2C, SPI, GPIO and the ADC. I would like to have a printf() available for debugging, too.

1. where can I find working examples for LPC844 for Keil? Are they available? I can't see them in the pack installer.

2. what library stack should I work with? My first and only priority is development speed. So it must be intuitive and well documented.

- CMSIS

- NXP libraries from examples

- FSL libraries from examples

- ??

I'm using Keil UVision MDK 5.33, Segger J-Link debug probe on Windows 10.

 

Thanks!

0 Kudos
Reply
5 Replies

2,880 Views
KoComputes
Contributor II

Thank you. How can I install the SDK files ?

It is not a uVision software pack. I made sure that 'Keil' was selected.

0 Kudos
Reply

2,868 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Under SDK there is Getting Started with MCUXpresso SDK.pdf

Have a look on this chapter: Run a demo using Keil® MDK/μVision

This will tell you how to run a Keil demo.

 

Have a nice day,

Jun Zhang

0 Kudos
Reply

2,849 Views
KoComputes
Contributor II

Thank you. I wasn't aware that guides for Keil are part of the MCUXpresso SDK documentation.

I got the examples working. Nice, very helpful.

Regarding the second part of my question: I will go with the fsl_ drivers, the CMSIS software pack, and study CMSIS and the SDK docs first.

0 Kudos
Reply

2,844 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Good to know. You are welcome!

0 Kudos
Reply

2,887 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

we have MCUXpresso SDK for Keil. 

Here is the download site: https://mcuxpresso.nxp.com/en/builder?hw=LPC844

ZhangJennie_0-1616051930942.png

 

Have a nice day

Jun Zhang

 

0 Kudos
Reply