LPC832: MRT_DisableInterrupts() doesn't actually prevent interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC832: MRT_DisableInterrupts() doesn't actually prevent interrupt

4,037件の閲覧回数
aaronm
Contributor IV

Hi, I'm using MRT on LPC832 (SDK: 2.16.000), and if I call the following, the interrupt for channel 1 does actually happen, and the flags for RUN and INT are set.  To ignore channel 1, I have to test for MRT_GetEnabledInterrupts() in the interrupt handler.  Which is Ok, because it works, but it seems counter-intuitive that if I say "disable interrupts for channel 1," the interrupt is still actually enabled.  Or am I doing something wrong?

Thanks!

 

 

void MRT0_DriverIRQHandler(void)
{
	if ( MRT_GetStatusFlags( MRT0, kMRT_Channel_0 ) == (MRT_CHANNEL_STAT_INTFLAG_MASK | MRT_CHANNEL_STAT_RUN_MASK) ) {
		MRT_ClearStatusFlags( MRT0, kMRT_Channel_0, kMRT_TimerInterruptFlag );
		g_doPWM = 0;
		g_LED0 = !g_LED0;
		GPIO_PinWrite( g_pins[0].gpio.base, g_pins[0].gpio.port, g_pins[0].gpio.pin, g_LED0 );
	}

	if ( MRT_GetEnabledInterrupts( MRT0, kMRT_Channel_1 ) ) {
	if ( MRT_GetStatusFlags( MRT0, kMRT_Channel_1 ) == (MRT_CHANNEL_STAT_INTFLAG_MASK | MRT_CHANNEL_STAT_RUN_MASK) ) {
		MRT_ClearStatusFlags( MRT0, kMRT_Channel_1, kMRT_TimerInterruptFlag );

		g_doPWM = 0;
		g_LED1 = !g_LED1;
		GPIO_PinWrite( g_pins[3].gpio.base, g_pins[3].gpio.port, g_pins[3].gpio.pin, g_LED1 );
	}
	}

	SDK_ISR_EXIT_BARRIER;
}

/*
 * @brief   Application entry point.
 */
int main(void) {

	/* Init board hardware. */
	BOARD_InitBootPins();
	BOARD_InitBootClocks();
	BOARD_InitBootPeripherals();
#ifndef BOARD_INIT_DEBUG_CONSOLE_PERIPHERAL
	/* Init FSL debug console. */
	BOARD_InitDebugConsole();
#endif

	mrt_config_t defaultMRTConfig;
	MRT_GetDefaultConfig( &defaultMRTConfig );
	MRT_Init( MRT0, &defaultMRTConfig );

	MRT_SetupChannelMode( MRT0, kMRT_Channel_0, kMRT_RepeatMode );
	MRT_SetupChannelMode( MRT0, kMRT_Channel_1, kMRT_RepeatMode );

	MRT_UpdateTimerPeriod( MRT0, kMRT_Channel_0, MRTINTERVAL, 1 );
	MRT_UpdateTimerPeriod( MRT0, kMRT_Channel_1, SYSCLOCK, 1 );
 
	MRT_EnableInterrupts( MRT0, kMRT_Channel_0, kMRT_TimerInterruptEnable );
	MRT_DisableInterrupts( MRT0, kMRT_Channel_1, kMRT_TimerInterruptEnable );
	EnableIRQ( MRT0_IRQn );  /* Normally, this would be called in peripherals.c */

 

ラベル(1)
0 件の賞賛
返信
7 返答(返信)

3,788件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I did a simple test with the part of the code that you upload, but I need more information, could you open an Internal case put my name I will take it, because I need you share the whole project or the whole main.c. I think replay the same issue that you report on my board.

Let me know what you do.

Best regards,
Pavel

0 件の賞賛
返信

3,774件の閲覧回数
aaronm
Contributor IV

Hey, Pavel, the entire code base can be found here, but it's not that important, I guess.  I can work around it.  I just wanted to understand the "why" behind the way it works, since it's somewhat unintuitive, but since I can work around it, it's less critical, now.

https://community.nxp.com/t5/LPC-Microcontrollers/LPC832-Sample-project-for-using-MRT-to-generate-mo...

Feel free to close this one out.

0 件の賞賛
返信

4,008件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel and I will be supporting your case, I reviwed the example on the SDK LPCOpen on the IDE MCUXpresso and this use the next to active.

/* Enable the interrupt for the MRT */

NVIC_EnableIRQ(MRT_IRQn);

 

And on bellow of this there is

void NVIC_DisableIRQ(IRQn_Type IRQn)

Could you try with this.

 

I couldn't find the function of MRT_GetEnabledInterrupts.

Best regards,
Pavel

0 件の賞賛
返信

4,000件の閲覧回数
aaronm
Contributor IV

Hi Pavel,

NVIC_DisableIRQ() will definitely shut off the interrupt for MRT, but it will shut off *all* interrupts for MRT.  The LPC832 has 4 channels for MRT, and they're all enabled or disabled, with NVIC_EnableIRQ() or disable, as above.

However, in the MRT peripheral, there's a MRT_DisableInterrupts() that should, I assume, disable a particular MRT channel, as needed.  So if I configure two MRT channels, and then want to stop one of them, MRT_DisableInterrupts() should do that.  However, in the interrupt handler, 

 

 

MRT_GetStatusFlags( MRT0, kMRT_Channel_1 ) == (MRT_CHANNEL_STAT_INTFLAG_MASK | MRT_CHANNEL_STAT_RUN_MASK) )

 

 

returns true, even if channel 1 has had its interrupt disabled.  This following check in the ISR will block the ISR portion for channel 1 from executing, but I'm wondering why the channel was hardware triggered in the first place, if the channel was disabled.

 

 

if ( MRT_GetEnabledInterrupts( MRT0, kMRT_Channel_1 ) )

 

 

SDK documentation is here: https://mcuxpresso.nxp.com/api_doc/dev/4555/a00017.html#gafa8493a0faee1cc356da26ca99a54da8

Like I said, I can work around this, but I'm curious if this is how it's supposed to work.

0 件の賞賛
返信

3,975件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I'm using the SDK of LPCOpen on the MCUXpresso and that library is not added, where are you develop this? Could you share the source of this example?

Pavel_Hernandez_0-1730510974198.png

 

Best regards,
Pavel

0 件の賞賛
返信

3,926件の閲覧回数
aaronm
Contributor IV

Hi Pavel,

Sorry for the delay: I was out of town for the weekend.  I got the SDK from NXP's SDK Builder: https://mcuxpresso.nxp.com/en  

Go there, select "Select Board / Processor"; enter "LPC832," and then build your SDk.  Current version is 2.16.000.

Aaron

0 件の賞賛
返信

3,910件の閲覧回数
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, thanks for the information I was using the LPCOpen, I will download and reviewed.

Best regards,
Pavel

0 件の賞賛
返信