LPC82x touch Solution board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC82x touch Solution board

ソリューションへジャンプ
2,614件の閲覧回数
jun1
Contributor V

Hi.

1.

I purchased a board and stabbed USB, but nothing is displayed on the LCD. The screen of the USB drive pops up on the PC screen.
Do you have any board settings?

2.

AN11622 LPC82x Touch Solution Quick Start Guide is a copy of the latest firmware (stand-alone demo software).
Where can I download the LPC82x Touch Solution's Standalone Demo (without GUI) bin file?

in trouble.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,804件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jun

in this url under "Software",  There is AN11620 source code 0 and LPC82x Touch Solution Lib V0101

LPC82x Touch Solution | NXP 

Please check if those files can help you.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,805件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jun

in this url under "Software",  There is AN11620 source code 0 and LPC82x Touch Solution Lib V0101

LPC82x Touch Solution | NXP 

Please check if those files can help you.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,804件の閲覧回数
jun1
Contributor V

thank you for your answer.

I saw it and downloaded it, but there was no source code 0.

So, I was looking for the next question.

https://community.nxp.com/thread/482337
LPC 82x touch solution can not return touch pads number

Download AN11620_source_code_0.zip, start IAR and rewrite include file path etc.

I was able to write to the board successfully.

Thank you very much.

jun

0 件の賞賛
返信