LPC82x.h missing ADC definitions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC82x.h missing ADC definitions

1,441件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjm on Mon Jan 19 02:30:03 MST 2015
According to my experience, most of the lpc8xx.h is okay for LPX82x series. But ADC resources (specific to 82x-subfamily) are missing there.

I'd suggest that updated header files are present, since the 82x is avaiable. It is not included in current LPCxpresso. Please answer ASAP, because of ongoing software development.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,384件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjm on Mon Jan 19 03:37:25 MST 2015
Thanks,
seems that this is OK. Until now, I have been working with the CMSIS includes.
0 件の賞賛
返信

1,384件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jan 19 02:40:02 MST 2015
All the headers are in the LPCOpen project for 824 (Hint: Look in the LPCOpen folder inside the Examples)
0 件の賞賛
返信