LPC82x.h missing ADC definitions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC82x.h missing ADC definitions

1,450 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjm on Mon Jan 19 02:30:03 MST 2015
According to my experience, most of the lpc8xx.h is okay for LPX82x series. But ADC resources (specific to 82x-subfamily) are missing there.

I'd suggest that updated header files are present, since the 82x is avaiable. It is not included in current LPCxpresso. Please answer ASAP, because of ongoing software development.
Labels (1)
0 Kudos
Reply
2 Replies

1,393 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rjm on Mon Jan 19 03:37:25 MST 2015
Thanks,
seems that this is OK. Until now, I have been working with the CMSIS includes.
0 Kudos
Reply

1,393 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Jan 19 02:40:02 MST 2015
All the headers are in the LPCOpen project for 824 (Hint: Look in the LPCOpen folder inside the Examples)
0 Kudos
Reply