LPC82x dma trigger outputs need clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC82x dma trigger outputs need clarification

1,276 Views
chrisgullentops
Contributor I

In OM10800 (the manual the LPC82x) under 12.3.2 there is a short description of the use of the DMA output triggers.

This is clear but does not bring mush info about how to set up the triggered channel in terms of settings of the channel configuration register.  One can assume that the output trigger is a pulse, firing when the channel descripter is exhausted. One can then also assume that the channel must be programmed for HW trigger in edge mode, and probably rising edge. But this is guessing. I prefer a more formal description

Labels (1)
0 Kudos
Reply
1 Reply

1,137 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chris Gullentops,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

The DMA trigger out is not assigned to output via pins, it's the internal connection.

It's ok for you to consider as the trigger signal and it would happen when the channel descriptor is exhausted.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply