LPC82x dma trigger outputs need clarification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC82x dma trigger outputs need clarification

1,263件の閲覧回数
chrisgullentops
Contributor I

In OM10800 (the manual the LPC82x) under 12.3.2 there is a short description of the use of the DMA output triggers.

This is clear but does not bring mush info about how to set up the triggered channel in terms of settings of the channel configuration register.  One can assume that the output trigger is a pulse, firing when the channel descripter is exhausted. One can then also assume that the channel must be programmed for HW trigger in edge mode, and probably rising edge. But this is guessing. I prefer a more formal description

ラベル(1)
0 件の賞賛
返信
1 返信

1,124件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Chris Gullentops,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

The DMA trigger out is not assigned to output via pins, it's the internal connection.

It's ok for you to consider as the trigger signal and it would happen when the channel descriptor is exhausted.

Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信