LPC82x Internal Voltage Ref to ADC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC82x Internal Voltage Ref to ADC?

1,272 Views
mwp_nxp
Contributor III

Hi all,

(I thought I posted this question yesterday, but it seem to have disappeared. Weird.)

The LPC82x has an internal 0.9v voltage reference that the doc's state can be used as a reference input to the comparator peripheral.

Is it possible for this reference to be routed to an ADC input?

I ideally would like to be able to measure it with the ADC, so I can then determine the VREFP (and so VDD) voltages. I have done this with MKL03/05 in the past.

Thankyou!

 

0 Kudos
Reply
1 Reply

1,261 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @mwp_nxp,

Unfortunately, there is not an option for routing the 0.9V internal bandgap reference voltage to an ADC input channel for the LPC84x.

As a recommendation, you could try reading the following Application Notes:

They might be useful.

Best regards, Raul.

0 Kudos
Reply