LPC824M201JHI33 use without oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC824M201JHI33 use without oscillator

844 次查看
daniel2
Contributor I
0 项奖励
回复
1 回复

774 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Daniel Brown

In the user manual of the LPC824 (https://www.nxp.com/docs/en/user-guide/UM10800.pdf) under section 5.3.2 you can find the following information. 

pastedImage_4.png

So, you can definitely use the internal oscillator as the main clock. The development board for the LPC824 (LPCXpresso824-MAX Board for LPC82x family MCUs|NXP ) actually uses the IRC in all the examples that we provide (Code Bundle, LPCOpen and SDK) as the input for the PLL and the output of the PLL is the source of the main clock.

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 项奖励
回复