LPC824M201JDH20,we want to save some data into flash ,and how to read and write flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824M201JDH20,we want to save some data into flash ,and how to read and write flash?

726件の閲覧回数
wensinnywen
Contributor I

we are using LPC824M201JDH20, the demo "flashiap" has no read method,  we want to save some data into flash ,and how to read and write flash? 

タグ(1)
0 件の賞賛
返信
1 返信

649件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Wen sinnywen,

    flashiap demo already have the write flash function, just the program flash function.

   Flash program and erase need to use the IAP function to realize it, but the read is very simple, just read the address directly.

   Read operation is:

variable= (uint32_t *)(address);

Take an example:

#define LONGWORD_COUNTER_ADDR 0x14000040
#define WORD_COUNTER_ADDR 0x14000044
#define BYTE_COUNTER_ADDR 0x14000046

                printf("\nlongword counter = 0x%08X", *(uint32 *)(LONGWORD_COUNTER_ADDR));
              printf("\nword counter = 0x%04X", *(uint16 *)(WORD_COUNTER_ADDR));
              printf("\nbyte counter = 0x%02X", *(uint8 *)(BYTE_COUNTER_ADDR));

Wish it helps you!

If you still have question about it, please kindly let me know.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信