LPC824 WITH MQTT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC824 WITH MQTT

2,650件の閲覧回数
aravindpb5009
Contributor III

HAI 

     I am  using LPC824  ,mcuxpresso ide now i am using usart communication for transmitting the data but future planned to send the data through MQTT format , please give some idea  how to send MQTT data and MQTT format on our LPC824

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

2,481件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Aravind,

As far as I know that the MQTT data are transferred via Ethernet based on TCP/IP or WIFI, tbut the LPC824 does not have Ethernet module. Do you have WIFI or Ethernet controller?

We have AWS example based on SDK package for example LPC546xx, pls download the SDK and refer to the AWS example.

Welcome | MCUXpresso SDK Builder 

BR

Xiangjun Rong

0 件の賞賛
返信

2,481件の閲覧回数
aravindpb5009
Contributor III

i am using wifi module 

0 件の賞賛
返信