LPC824 SPI Master using DMA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824 SPI Master using DMA

2,570 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tobias2504 on Tue Apr 19 08:12:36 MST 2016
Hi,

Im trying to get SPI as Master using DMA to run on a LPC824. SPI in polling mode as well in interrupt mode is working but not DMA.

#include "chip.h"

/******************************************************************************
 * Defines
 *****************************************************************************/
#define INTERRUPT 1
#defineDMA1

#define SPI_BUFFER_SIZE 64


/******************************************************************************
 * Global Variables
 *****************************************************************************/
static uint16_t txBuf[SPI_BUFFER_SIZE];
static uint16_t rxBuf[SPI_BUFFER_SIZE];

static SPI_DATA_SETUP_T tx0Setup;


/******************************************************************************
 * Routines
 *****************************************************************************/
void SPI0_IRQHandler(void)
{
// Disable SPI0 Interrupts
Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENSET_TXDYEN | SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN, DISABLE);

if(tx0Setup.TxCnt < tx0Setup.Length)
{
Chip_SPI_Int_RWFrames(LPC_SPI0,&tx0Setup);
Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENSET_TXDYEN | SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN, ENABLE);
}

// Get status flags
uint32_t status = Chip_SPI_GetStatus(LPC_SPI0);

// Clear status flags
Chip_SPI_ClearStatus(LPC_SPI0, status);
}

static void Init_SPI_PinMux(void)
{
// Enable the clock for the switch matrix controller
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_SWM);

// Assign a movable pin functions to a physical pins
Chip_SWM_MovablePinAssign(SWM_SPI0_SCK_IO, 16);
Chip_SWM_MovablePinAssign(SWM_SPI0_MOSI_IO, 27);
Chip_SWM_MovablePinAssign(SWM_SPI0_MISO_IO, 26);
Chip_SWM_MovablePinAssign(SWM_SPI0_SSEL0_IO, 15);

// Disable the clock for the switch matrix controller
Chip_Clock_DisablePeriphClock(SYSCTL_CLOCK_SWM);
}

/******************************************************************************
 * Start Routine
 *****************************************************************************/
int main(void)
{
volatile static int i = 0 ;

    // Read clock settings and update SystemCoreClock variable
    SystemCoreClockUpdate();

    // Setup buffers
for(i=0; i<SPI_BUFFER_SIZE; i++)
{
txBuf = i+1;
rxBuf = 0;
}

// Initialize SPI
    Init_SPI_PinMux();
Chip_SPI_Init(LPC_SPI0);
LPC_SPI0->CFG = (SPI_MODE_MASTER | SPI_CLOCK_CPHA0_CPOL0 | SPI_DATA_MSB_FIRST | SPI_SSEL_ACTIVE_LO);
Chip_SPI_Enable(LPC_SPI0);

// Initialize DMA
#if(DMA)
Chip_DMA_Init(LPC_DMA);
Chip_DMA_Enable(LPC_DMA);
Chip_DMA_SetSRAMBase(LPC_DMA, DMA_ADDR(Chip_DMA_Table));
Chip_DMA_SetupChannelConfig(LPC_DMA, DMAREQ_SPI0_TX, (DMA_CFG_PERIPHREQEN | DMA_CFG_TRIGBURST_SNGL | DMA_CFG_CHPRIORITY(3)));

Chip_DMA_Table[DMAREQ_SPI0_TX].source = DMA_ADDR(&txBuf[SPI_BUFFER_SIZE-1]);
Chip_DMA_Table[DMAREQ_SPI0_TX].dest = DMA_ADDR(&LPC_SPI0->TXDAT);
Chip_DMA_Table[DMAREQ_SPI0_TX].next = DMA_ADDR(0);
Chip_DMA_Table[DMAREQ_SPI0_TX].xfercfg= DMA_XFERCFG_CFGVALID | DMA_XFERCFG_SWTRIG | DMA_XFERCFG_WIDTH_8 | DMA_XFERCFG_SRCINC_1 | DMA_XFERCFG_DSTINC_0 | DMA_XFERCFG_XFERCOUNT(SPI_BUFFER_SIZE);

// Setup transfer descriptor and validate it
Chip_DMA_SetupTranChannel(LPC_DMA, DMAREQ_SPI0_TX, &Chip_DMA_Table[DMAREQ_SPI0_TX]);

// Setup data transfer --> Start Sending data?
Chip_DMA_SetupChannelTransfer(LPC_DMA, DMAREQ_SPI0_TX, Chip_DMA_Table[DMAREQ_SPI0_TX].xfercfg);

#else

// Setup SPI Transfer setup
tx0Setup.Length = SPI_BUFFER_SIZE;
tx0Setup.pTx = txBuf;
tx0Setup.pRx = rxBuf;
tx0Setup.RxCnt = tx0Setup.TxCnt = 0;
tx0Setup.DataSize = 8;

#if(INTERRUPT)
// Send SPI via interrupt mode
NVIC_EnableIRQ(SPI0_IRQn);
Chip_SPI_Int_RWFrames(LPC_SPI0, &tx0Setup);
Chip_SPI_Int_Cmd(LPC_SPI0, SPI_INTENSET_TXDYEN | SPI_INTENSET_RXDYEN | SPI_INTENSET_RXOVEN | SPI_INTENSET_TXUREN, ENABLE);
#else
// Send SPI via blocking mode
Chip_SPI_WriteFrames_Blocking(LPC_SPI0, &tx0Setup);
#endif

#endif

    // Enter an infinite loop
    while(1)
    {
        __WFI();
    }
    return 0 ;
}


Can anyone help me?

Thanks,
Tobi
Labels (1)
0 Kudos
Reply
2 Replies

1,987 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,987 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by tobias2504 on Wed Apr 20 00:23:12 MST 2016
Got it. I attached my example code for this.
0 Kudos
Reply