LPC824, PLL post divider is not working?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC824, PLL post divider is not working?

2,268 Views
rianzu
Contributor II

Hello,

 

After several hours of struggle and confusing manual, here is the problem on LPC824:

 

According to LPC82x User Manual, pag. 56, the PLL block have some high frequency oscillator (called CCO) that can work (can be locked) in FCCO = 156...320 MHz range.

 

After CCO, exists a post divider that can be set to 4 divider values (1,2,4 and 8) automatically further divided by 2 for 50 % duty-cycle, resulting in real P = 2,4,8 or 16. This is for obtaining FCLKOUT (MAIN CLOCK) that is limited to 100MHz.

 

To close the PLL loop, exists also a M divider (called feedback in user manual) that can be set such as real divider values = 1...32

 

Now when injecting 12 MHz from IRC into PLL and set M = 5, MAIN CLOCK will be 60 MHz with no effect of changing P value. That is, any value set to P the clock will be 60 MHz (IRC * M). Since FCCO can be locked only in 156...320 MHz range, we deduce that lock is produced at 240 MHz and real P is 4 (P = 2, 2*P = 4).

 

We enabled CLOCKOUT to monitor MAIN SYSTEM CLOCK and this indeed outputs 60 MHz, 72 MHz or whatever M is set to multiply the 12 MHz IRC.

 

Any value programmed in P bits (pag. 35, SYSPLLCTRL register) have no effect.

 

Taking example from table 57 (pag. 58) if keep M=5 and set P = 4 (real P = 8) the CCO should (still) lock on 240 MHz but MAIN CLOCK should be 30 MHz (well under 100 MHz limit). Instead, example keep the MAIN CLOCK = 60 MHz and modify the SYSTEM CLOCK from SYSAHBCLKDIV register.

 

Appears that P divider is just not working, and set at fixed value P = 2 (real P for PLL formula = 4) regarding PSEL bits setting in SYSPLLCTRL register.

 

Can someone confirm this?

Tnx,

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,748 Views
rolfmeeser
NXP Employee
NXP Employee

There's nothing wrong with the post divider!

M is the divider between output of the PLL block and the phase detector. Therefore, the PLL cannot but provide M times the reference frequency there.

Now the PLL adjusts the output frequency by changing the CCO clock frequency. The P divider ensures that the CCO can operate in its guaranteed frequency range. A 60 MHz output can only be achieved with a 240 MHz CCO, and the P divider ratio must be four. Your calculation is completely right!

Sometimes it is possible that the system works even with an incorrect P divider setting. Assume you want to get 90 MHz out. The correct CCO frequency is 180 MHz here (P divider ratio = 2), but it *might* still work with a P divider ratio of 4, as the resulting CCO frequency of 360 MHz is not too far out of the guaranteed operating window.

0 Kudos
Reply