LPC824 Max board xtal oscillator not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC824 Max board xtal oscillator not working

672 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ECamino on Wed May 04 13:10:18 MST 2016
Hi,

I removed 0-ohm resistors and solder-jumped SJ3 1&2 and SJ4 1&2. 

I have continuity on Y2 to pins 17 and 18.

Using LPCOpen project for LPC824 "periph_wwdt"

In file sysinit_8xx.c, line 68, comment "Chip_SetupIrcClocking();" and add line "Chip_SetupXtalClocking();" 

Build, run debug (using LPCLink on an LPCxpresso 800 board) and I can see it hangs at sysinit_8xx.c, line 78: "while (!Chip_Clock_IsSystemPLLLocked()){}"

I checked the Y2 signal with a scope, and there is no crystal signal from either Y2 pad.

What do I have to do to enable the crystal clock on an LPC824 Max board?

Thanks,

EC
标签 (1)
0 项奖励
回复
1 回复

559 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复