LPC822 ADC sequence wrong values

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC822 ADC sequence wrong values

1,753 次查看
miesalex
Contributor I

Hi,

I have a problem using the sequences of the LPC822.

When I select multiple channels to be read in a sequence and I select single step everything is fine and the correct values are read. However when disabling single step one channel (10)  gives me wrong values. The incorrect value is consistent though, it wil always be the same incorrect value.

Anyone got any idea what this could possibly be? Source code down below. A convertion is triggered manually by the MRT every 100ms.

Thx,

Alexander

void Init_adc(void)
{
/* Power up ADC and enable ADC clock */
Chip_SYSCTL_PowerUp(SYSCTL_SLPWAKE_ADC_PD);
Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_ADC);

/* Perform ADC calibration */
LPC_ADC->CTRL = ADC_CR_CLKDIV((SystemCoreClock / 500000) - 1) | ADC_CR_CALMODEBIT;
while((LPC_ADC->CTRL & ADC_CR_CALMODEBIT) != 0); // Wait until the CALLMODE bit clears

/* Set the ADC clock divider for maximum speed */
LPC_ADC->CTRL = ADC_CR_CLKDIV(0);

/* Configure SEQA as to read the current, temperature and voltage */
LPC_ADC->SEQ_CTRL[0] = ADC_SEQ_CTRL_CHANSEL(3) | ADC_SEQ_CTRL_CHANSEL(10) | ADC_SEQ_CTRL_CHANSEL(11);

/* Trigger polarity is positive edge */
LPC_ADC->SEQ_CTRL[0] |= ADC_SEQ_CTRL_HWTRIG_POLPOS;

/* Interrupt at end of sequence */
LPC_ADC->SEQ_CTRL[0] |= ADC_SEQ_CTRL_MODE_EOS;

/* Enable SEQA */
LPC_ADC->SEQ_CTRL[0] |= ADC_SEQ_CTRL_SEQ_ENA;

/* Enable interrupts for SEQA */

LPC_ADC->INTEN = ADC_INTEN_SEQA_ENABLE;
NVIC_EnableIRQ(ADC_SEQA_IRQn);
}

void ADC_SEQA_IRQHandler(void)
{

state.current = CONVERT_ADC_CURRENT(ADC_DR_RESULT(LPC_ADC->DR[3]));
state.temperature = CONVERT_ADC_TEMPERATURE(ADC_DR_RESULT(LPC_ADC->DR[10]));
state.voltage = CONVERT_ADC_VOLTAGE(ADC_DR_RESULT(LPC_ADC->DR[11]));
}

标签 (1)
标记 (2)
1 回复

1,419 次查看
wernerf
Contributor II

Hi Alexander,

you have chosen to generate ADC interrupts at the end of every sequence of conversions.

In this case you need to clear the SEQA_INT flag by software in the interrupt handler.

You need to set :smileyalert: bit 28 in the LPC_ADC->FLAGS register.

pastedImage_1.png