LPC820 Pinmuxing tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC820 Pinmuxing tool

1,286 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Mon Oct 06 13:38:54 MST 2014
The LPC Initialization pinmux tool now supports the LPC820 parts.

You can configure the switch matrix, IOCON and INMUX for the LPC822 and LPC824 parts here:

LPC Initializer and pinmux tool

The tool provides a simple to use interface for assigning signals to pins. It generates C source code which can be dropped straight into your LPC Open project.

Watch this video tutorial for pinmuxing with the LPC812 to familiarize yourself with the tool.
Video tutorial for LPC812

The tool support these targets:
[list]
  [*]LPC81x
  [*]LPC82x
  [*]LPC11E6x
  [*]LPC11U6x
  [*]LPC15xx
[/list]
Labels (1)
0 Kudos
Reply
1 Reply

1,232 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larsen on Thu Oct 16 15:56:09 MST 2014
Suggestion: When a pin has been assigned to a peripheral, it turns darker green. Fine - but I would suggest that the corresponding terminal on the focal peripheral also change colour to indicate that it has been assigned as well. As of now it does not change colour. Different colour would make the lpc-initializer easier to use.
0 Kudos
Reply