LPC81x UID Register Address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC81x UID Register Address

Jump to solution
4,581 Views
jose_oga
NXP Employee
NXP Employee

Hello Everyone,

Is there any way in which I can read unique 128-bit ID from the LPC81x directly from a memory register?

My application is using SWD connection for writing/reading the registers and using IAP would make the process much more complex.

I haven't been able to find the address of the UID on the User Manual, examples, or anywhere else.

Thanks!

0 Kudos
Reply
1 Solution
4,379 Views
gerhardk
Contributor II

Read four words from 0x0C000080

View solution in original post

6 Replies
4,379 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jose Ogando,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To my knowledge, the UID register address is not public, so IAP command is the best method to read the UID register.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
4,379 Views
jose_oga
NXP Employee
NXP Employee

Thanks for the quick response!

You mention that IAP command is the best method. Are there any other options?

Thanks!

0 Kudos
Reply
4,380 Views
gerhardk
Contributor II

Read four words from 0x0C000080

4,379 Views
theophileleroy
NXP Employee
NXP Employee

Where can I find this address for LPC802 ?

0 Kudos
Reply
4,379 Views
jose_oga
NXP Employee
NXP Employee

This seems to be working.

Thanks a lot!

0 Kudos
Reply
4,379 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jose Ogando,

1) Are there any other options?
-- I'm afraid it doesn't have other option

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply