LPC81x UID Register Address

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC81x UID Register Address

ソリューションへジャンプ
4,808件の閲覧回数
jose_oga
NXP Employee
NXP Employee

Hello Everyone,

Is there any way in which I can read unique 128-bit ID from the LPC81x directly from a memory register?

My application is using SWD connection for writing/reading the registers and using IAP would make the process much more complex.

I haven't been able to find the address of the UID on the User Manual, examples, or anywhere else.

Thanks!

0 件の賞賛
返信
1 解決策
4,606件の閲覧回数
gerhardk
Contributor II

Read four words from 0x0C000080

元の投稿で解決策を見る

6 返答(返信)
4,606件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jose Ogando,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To my knowledge, the UID register address is not public, so IAP command is the best method to read the UID register.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
4,606件の閲覧回数
jose_oga
NXP Employee
NXP Employee

Thanks for the quick response!

You mention that IAP command is the best method. Are there any other options?

Thanks!

0 件の賞賛
返信
4,606件の閲覧回数
gerhardk
Contributor II

Read four words from 0x0C000080

4,606件の閲覧回数
theophileleroy
NXP Employee
NXP Employee

Where can I find this address for LPC802 ?

0 件の賞賛
返信
4,606件の閲覧回数
jose_oga
NXP Employee
NXP Employee

This seems to be working.

Thanks a lot!

0 件の賞賛
返信
4,606件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Jose Ogando,

1) Are there any other options?
-- I'm afraid it doesn't have other option

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信