LPC812 - Target marked as not debuggable

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC812 - Target marked as not debuggable

1,955件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by masterboy on Wed Dec 11 03:23:00 MST 2013
Can anyone advise me how to unlock the processor? When recording the program to the processor occurs error:

[color=#f00]Failed on connect: Ep(01). Target marked as not debuggable.
Conn&Reset. Was: None. DpID:  BC11477. Info: HID64HS12[/color]


I tried to delete the program using ISP, but I can not run this mode. Is the lpc812 dead?
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vijay_nav on Tue Jan 07 04:06:13 MST 2014
Hai
       I am facing the same problem while debugging and i have followed the link but i am not able to understand.will any one clear explain how to solve the problem.Some said that ISP handler but i dont now where exactly the ISP handle is please explain me clearly.


Thanks in advance. 
0 件の賞賛
返信

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by masterboy on Mon Dec 16 04:20:36 MST 2013

Quote: lpcxpresso-support
There is a FAQ on this:
http://www.lpcware.com/content/faq/lpcxpresso/target-marked-not-debuggable



Thank you. The mistake was on my side :) ISP handler was on pin PIO0_12 not PIO0_1 as usual.
0 件の賞賛
返信

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 11 03:25:57 MST 2013
There is a FAQ on this:
http://www.lpcware.com/content/faq/lpcxpresso/target-marked-not-debuggable
0 件の賞賛
返信