LPC811 debug "No source available" error.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC811 debug "No source available" error.

1,572 Views
jkingeet
Contributor I

Trying to use LPCXpresso v8.1.4 to program an LPC811 via LPC-Link probe v1.3.

Results in "No source available for "0x1fff0008" error message.


Reading the UM, the 0x1fff0000 memory space is related to the bootloader mode.
Researching, I found a past forum post that suggested this sort of issue may stem from the processor being in ISP mode.
According to the UM, ISP entry pin can be either PIO0_1 or PIO0_12 (depending on the marking and bootloader version, neither or which do I know how to verify).
The specific name of the processor that I am using is LPC811M001JDH16, which, according to a different section of the UM, uses ISP entry pin PIO0_12 (physical pin 2).
I added an external pull-up resistor to VDD on this pin to avoid ISP entry.

PIO0_1 in my application is tied to an external, 24MHz clock signal.

 

I'm at a loss for where to look next.
Does anyone have thoughts on this issue?

Copy-pasted from my post in the LPCXpresso-IDE community for exposure to both groups.

Labels (1)
0 Kudos
Reply
1 Reply

1,205 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Justin King,

    This question has been answered in your another post:

LPC811 debug "No source available" error. 

   I find your problem is solved by updating the LPCXpresso IDE to the latest version.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply