LPC810 Question about connect ACMP_O to SCT input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC810 Question about connect ACMP_O to SCT input

909 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by [email protected] on Wed Jun 26 05:38:20 MST 2013

<span class="postbody">User manual states:
You can use the comparator output function (ACMP_O) to start or stop the SCT or, more
generally, create an SCT event. To create an SCT event, connect AMP_O as follows:
1. Using the switch matrix, connect ACMP_O to a pin. See Table 203.
2. Using the switch matrix, connect any of the SCT input functions to the same pin.
See Table 107.
The selected SCT input can now monitor the ACMP_O function.

My question now is: do i have to use a real exsiting pin or it is possible to use i.e. P0.6 which is physical not connected to a external pin ?
</span><span class="postbody">This would save a physical pin carry a signal i dont need to connect outside of the MCU.</span>

Labels (1)
0 Kudos
Reply
1 Reply

898 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Paul on Wed Aug 14 14:27:59 MST 2013
It is never a good idea to use a pin that does not exist in the device data sheet.  Although it may work in some situations, there is no guarantee that it will continue to function correctly in future device revisions.
0 Kudos
Reply