LPC804 Writing into Flash memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC804 Writing into Flash memory

跳至解决方案
3,357 次查看
ashokfair
Contributor IV

Hi Everyone,

Im currently using the SDK Version: KSDK 2.4.1 (2018-06-18) for LPC804 ,

Please help me to write data in Flash memory , im not finding any example for the same.

Thanks,

Ashok

标签 (1)
0 项奖励
回复
1 解答
3,116 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,117 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

0 项奖励
回复
3,116 次查看
ashokfair
Contributor IV

Hi Alexis,

Thank you so much. I tested the code with LPC804 and working fine and verified OK  :smileyhappy:

pastedImage_3.png

Thanks,

Ashok R

0 项奖励
回复
2,469 次查看
BerlinRaj
Contributor II

dear ashok, can you please post how to read the value from the flash memory ?

0 项奖励
回复