LPC804 Writing into Flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC804 Writing into Flash memory

Jump to solution
3,395 Views
ashokfair
Contributor IV

Hi Everyone,

Im currently using the SDK Version: KSDK 2.4.1 (2018-06-18) for LPC804 ,

Please help me to write data in Flash memory , im not finding any example for the same.

Thanks,

Ashok

Labels (1)
0 Kudos
Reply
1 Solution
3,154 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

View solution in original post

0 Kudos
Reply
3 Replies
3,155 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Ashok Ra,

Here is an example for writing in flash memory for the LPC802, it should work in the LPC804 too.

Hope it helps,

Alexis Andalon

0 Kudos
Reply
3,154 Views
ashokfair
Contributor IV

Hi Alexis,

Thank you so much. I tested the code with LPC804 and working fine and verified OK  :smileyhappy:

pastedImage_3.png

Thanks,

Ashok R

0 Kudos
Reply
2,507 Views
BerlinRaj
Contributor II

dear ashok, can you please post how to read the value from the flash memory ?

0 Kudos
Reply