LPC804 SPI SBL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC804 SPI SBL

1,841 Views
redwolf
Contributor I

Hi everyone,

I have a project based on LPC804 and I'm trying to flash it with lpc804_spi_sbl  keil project like in AN12378 example. Unfortunately I didn't manage to make the keil project work, there are many errors due to the incompatibility with newer version of compiler(Arm Compiler 5 & 6). Is there a more recent version of this example? Maybe one for MCUXpresso IDE/ vs code?

Thank you!

Labels (1)
0 Kudos
Reply
2 Replies

1,823 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, the information on the page is the last information available.

LPC80x 15 MHz|Arm Cortex-M0+|32-bit Microcontrollers (MCUs) | NXP Semiconductors

Pavel_Hernandez_0-1716238372286.png

Best regards,
Pavel

1,805 Views
redwolf
Contributor I

Thank you!

0 Kudos
Reply