LPC802 dev/evk board - where can I get the example application source code ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC802 dev/evk board - where can I get the example application source code ?

跳至解决方案
1,209 次查看
paulw2
Contributor III

Hi,

I'd like to work through the source code of the example application that the LPC802 dev kit has pre-installed.

This is the app that reads the temperature sensor, potentiometer, etc and lights LED's in a face pattern.

This source code would seem to be an excellent starting point as it's interfacing with most peripherals on the board.

I have the SDK installed but it doesn't seem to contain the source code for this example app.

Internet searches refer to example bundles, but I can't find one for LPC802 dev board.

Where can I get the LPC802 dev/evk board example application source code ?

Thanks in advance.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,117 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @paulw2 

The LPC802 dev/evk board example application source code is in the attachment.

Please kindly check it.

Hope this will help you.

BR

Hang

在原帖中查看解决方案

2 回复数
1,118 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @paulw2 

The LPC802 dev/evk board example application source code is in the attachment.

Please kindly check it.

Hope this will help you.

BR

Hang

938 次查看
paulw2
Contributor III
Hi Hang,

Apologies for very late reply.

Thank you very much for providing this.
0 项奖励
回复