LPC802 dev/evk board - where can I get the example application source code ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC802 dev/evk board - where can I get the example application source code ?

Jump to solution
2,110 Views
paulw2
Contributor III

Hi,

I'd like to work through the source code of the example application that the LPC802 dev kit has pre-installed.

This is the app that reads the temperature sensor, potentiometer, etc and lights LED's in a face pattern.

This source code would seem to be an excellent starting point as it's interfacing with most peripherals on the board.

I have the SDK installed but it doesn't seem to contain the source code for this example app.

Internet searches refer to example bundles, but I can't find one for LPC802 dev board.

Where can I get the LPC802 dev/evk board example application source code ?

Thanks in advance.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,017 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @paulw2 

The LPC802 dev/evk board example application source code is in the attachment.

Please kindly check it.

Hope this will help you.

BR

Hang

View solution in original post

2 Replies
2,018 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @paulw2 

The LPC802 dev/evk board example application source code is in the attachment.

Please kindly check it.

Hope this will help you.

BR

Hang

1,838 Views
paulw2
Contributor III
Hi Hang,

Apologies for very late reply.

Thank you very much for providing this.
0 Kudos
Reply