[LPC802] Periodic peak current during LOW power down

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[LPC802] Periodic peak current during LOW power down

2,669件の閲覧回数
emmanuelJJ
Contributor I

Hi All,

I have configured my LPC802 as following before entering in power down mode

- FRO set to 9MHz and set as main clock

- LPOSC_PD is powered and BOD_PD is powered down in PDSLEEPCFG

- Only ACMP is powered down in  PDRUNCFG and PDAWAKECFG

- All interrupts wake-up are disabled ==> STARTERP1 and STARTERP0 have the reset value

- All the peripheral  clock are disable in SYSAHBCLKCTRL. Except  for SYS, ROM, RAM0, Flash

- WKT and WDT clock are disabled in LPOSCCLKEN

- PM set to 0x2

- Write one to the SLEEPDEEP bit in the Arm Cortex-M0+ SCR register

- Use the Arm WFI instruction

With all this configuration, I have a periodic peak current of 5mA each 30ms when watching Power Measurement window.

 

It looks like something is running in back ground.

Any idea?

 

Thank a lot for your support.

 

Best regards,

 

Emmanuel

 

 

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,659件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

 

How about run the power_mode_switch_lpc demo under SDK, does it also have periodic peak current of 5mA each 30ms ? 

And what is wake-up source in your project?

 

BR

Alice

0 件の賞賛
返信

2,656件の閲覧回数
emmanuelJJ
Contributor I

Hi Alice,

1) I don't test demo under SDK.

2) There isn't wake-up source. Everything are disable

 

Best regards

 

Emmanuel

0 件の賞賛
返信

2,645件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello emmanuelJJ,

 

Sorry just from your first description it hard to identify the problem.

 

BR

Alice

0 件の賞賛
返信