LPC800 ISP commands conflict with LPC1800 ISP commands

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC800 ISP commands conflict with LPC1800 ISP commands

596件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MarcVonWindscooting on Wed Jul 31 05:24:42 MST 2013
Dear NXP developers,

you must be joking, when using the same command code 'S' for 'read CRC check[u]s[/u]um on' LPC800 and for '[u]s[/u]et active boot flash bank' on LPC1800 |(
There aren't any charaters left, are there?

They do differ in parameter count at least, but I would not count on the LPC1800 ISP handler to reject S 0 1024\r\n for example...

Why not use 'X' for set eXecutable bank on LPC1800 or 'H' for Hash sum on LPC800. Or maybe use lowercase 's' for the less dangerous command
'checksum' LPC800 and for
ラベル(1)
0 件の賞賛
返信
0 返答(返信)