LPC55xx with external clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55xx with external clock

2,740 Views
otsl
Contributor III

The datasheet for the LPC55S6x states that an external clock can be used on the XTAL32M_P pin if the clock is a square wave from 0V to 850mV.  Can someone elaborate on this? What is the tolerance of "0" and "850mV"?  Is a DC offset acceptable as long as the amplitude is 850mVpp? Is 850mV the absolute maximum for the the pin?

Previous LPC parts allowed an external oscillator to be capacitor divided and driven into the XTALIN pin, but that process will not guarantee a 0-850mV signal from a 3.3V oscillator (there will be some DC offset).  Without a little more information (or a recommended circuit) it is near impossible to design a robust system.

Labels (1)
0 Kudos
Reply
3 Replies

2,727 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

DC offset is not acceptable as long as the amplitude is 850mVpp.
850mV is the absolute maximum for the the pin.
this pin absolute input range is 0-850mV.

Have a nice day

Jun Zhang

 

Best Regards

Jun Zhang

0 Kudos
Reply

2,692 Views
otsl
Contributor III

Thank you Jun. Can you also provide the minimum amplitude that will reliably be detected?

0 Kudos
Reply

2,681 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

We don't have this minimum amplitude data.

But based on practice, I suggest you make sure the amplitude over 100mV.

 

Have a nice day

Jun Zhang

0 Kudos
Reply