LPC55xx with external clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55xx with external clock

2,780 次查看
otsl
Contributor III

The datasheet for the LPC55S6x states that an external clock can be used on the XTAL32M_P pin if the clock is a square wave from 0V to 850mV.  Can someone elaborate on this? What is the tolerance of "0" and "850mV"?  Is a DC offset acceptable as long as the amplitude is 850mVpp? Is 850mV the absolute maximum for the the pin?

Previous LPC parts allowed an external oscillator to be capacitor divided and driven into the XTALIN pin, but that process will not guarantee a 0-850mV signal from a 3.3V oscillator (there will be some DC offset).  Without a little more information (or a recommended circuit) it is near impossible to design a robust system.

标签 (1)
0 项奖励
回复
3 回复数

2,767 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

DC offset is not acceptable as long as the amplitude is 850mVpp.
850mV is the absolute maximum for the the pin.
this pin absolute input range is 0-850mV.

Have a nice day

Jun Zhang

 

Best Regards

Jun Zhang

0 项奖励
回复

2,732 次查看
otsl
Contributor III

Thank you Jun. Can you also provide the minimum amplitude that will reliably be detected?

0 项奖励
回复

2,721 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

We don't have this minimum amplitude data.

But based on practice, I suggest you make sure the amplitude over 100mV.

 

Have a nice day

Jun Zhang

0 项奖励
回复