LPC55xx GPIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55xx GPIO

2,804件の閲覧回数
ianbenton
Senior Contributor I

Are the GPIO inputs 5V tolerant?
If not, are there protection diodes from input to Vdd and Vss, so that it would be possible to connect a 5V input simply by using a current limiting resistor and allowing the upper protection diode to conduct (as is normally done in logic gates)?

0 件の賞賛
返信
4 返答(返信)

2,792件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello ianbenton,

The LPC55XX GPIOs are not 5V tolerant. Only the VBUS pin is 5V tolerant. For more details please refer to the LPC55XX Datasheet.

My apologies for the inconvenience.

Regards,
Gustavo

0 件の賞賛
返信

2,789件の閲覧回数
ianbenton
Senior Contributor I

Not inconvenient if I find out now.

Only inconvenient if I find out AFTER I've made my pcb.

I don't see any spec for the maximum current through the protection diode.

Also, the spec implies that the maximum voltage on a GPIO pin is 3.6V regardless of the value of Vdd. i.e  the pin could be taken 1.8V above Vdd if Vdd were 1.8V.

Is this correct?

0 件の賞賛
返信

2,787件の閲覧回数
ianbenton
Senior Contributor I

Found the maximum voltage spec elsewhere in the datasheet, but not the maximum current through the protection diodes.

0 件の賞賛
返信

2,777件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello ianbenton,

The maximum current trough the protection diodes is not characterized in the datasheet. There are some pin static characteristics including input current which would be the recommended limit.

Regards,
Gustavo

0 件の賞賛
返信