LPC55s69 multiple voltage levels

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55s69 multiple voltage levels

ソリューションへジャンプ
977件の閲覧回数
hazarm
Contributor I

hi,

is it possible to power the lpc55s69 rails as :

VBAT_DCDC = 1.8V
VBAT_PMU= 1.8V
VDDx =  1.8V

VDDA= 3.3V
VREFP= 3.3V


thank you in advance,
best,

hazar

 

ラベル(1)
0 件の賞賛
返信
1 解決策
935件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I get reply, it is not allowed and VDDA and VREFP are connected to 3.3V, while the digital power supply VBAT_DCDC, VBAT_PMU and VDD are connected to 1.8V for LPC55xx.

 

This is AE reply:

"

I'm assuming customer wants to use 3.3V VREFP and VDDA for measuring analog voltages greater than 1.8V.

Before we can assess whether the VDDA and VREFP can exceed the VDD/VBAT_PMU/VBAT_DCDC supply voltages, the voltage applied to any IO can not exceed (VDD + 0.5V) as specified by limiting values (DS Table 11). So in theory, the analog voltage shall not exceed 2.3V when VDD is powered using 1.8V supply, no matter whether the ADC part and VREF is powered by 3.3V. Please refer to the pad structure described in the UM11126, figure 49 for ESD clamping diode connections on the IO pad.

Another issue while powering the device with 1.8V: Please note that 1.8V is the absolute minimum voltage for device to functional normally, so powering the device with an 1.8V regulator may exceed the operational range of the device, either transiently or constantly.

 

Also, there's a note in the pin description which requires VDDA tied to VBAT_PMU/VBAT_DCDC, so the customer's setup is a direct violation of the following requirement described in DS table 3, and since VREFP's maximum voltage is VDDA, so it's not possible using 1.8V to power the VBAT_PMU/VBAT_DCDC/VDD while using 3.3V to power the VDDA and VREFP:

xiangjun_rong_0-1708499801188.png

 

In general, we do not recommend powering the VDDA using a separate power rail on LPC55S69.

"

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
960件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I will confirm with AE team if it is okay that VDDA is greater than VDD and VBAT_DCDC.

BR

XiangJun Rong

0 件の賞賛
返信
936件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I get reply, it is not allowed and VDDA and VREFP are connected to 3.3V, while the digital power supply VBAT_DCDC, VBAT_PMU and VDD are connected to 1.8V for LPC55xx.

 

This is AE reply:

"

I'm assuming customer wants to use 3.3V VREFP and VDDA for measuring analog voltages greater than 1.8V.

Before we can assess whether the VDDA and VREFP can exceed the VDD/VBAT_PMU/VBAT_DCDC supply voltages, the voltage applied to any IO can not exceed (VDD + 0.5V) as specified by limiting values (DS Table 11). So in theory, the analog voltage shall not exceed 2.3V when VDD is powered using 1.8V supply, no matter whether the ADC part and VREF is powered by 3.3V. Please refer to the pad structure described in the UM11126, figure 49 for ESD clamping diode connections on the IO pad.

Another issue while powering the device with 1.8V: Please note that 1.8V is the absolute minimum voltage for device to functional normally, so powering the device with an 1.8V regulator may exceed the operational range of the device, either transiently or constantly.

 

Also, there's a note in the pin description which requires VDDA tied to VBAT_PMU/VBAT_DCDC, so the customer's setup is a direct violation of the following requirement described in DS table 3, and since VREFP's maximum voltage is VDDA, so it's not possible using 1.8V to power the VBAT_PMU/VBAT_DCDC/VDD while using 3.3V to power the VDDA and VREFP:

xiangjun_rong_0-1708499801188.png

 

In general, we do not recommend powering the VDDA using a separate power rail on LPC55S69.

"

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信