LPC55s69 multiple voltage levels

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s69 multiple voltage levels

Jump to solution
859 Views
hazarm
Contributor I

hi,

is it possible to power the lpc55s69 rails as :

VBAT_DCDC = 1.8V
VBAT_PMU= 1.8V
VDDx =  1.8V

VDDA= 3.3V
VREFP= 3.3V


thank you in advance,
best,

hazar

 

Labels (1)
0 Kudos
Reply
1 Solution
817 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I get reply, it is not allowed and VDDA and VREFP are connected to 3.3V, while the digital power supply VBAT_DCDC, VBAT_PMU and VDD are connected to 1.8V for LPC55xx.

 

This is AE reply:

"

I'm assuming customer wants to use 3.3V VREFP and VDDA for measuring analog voltages greater than 1.8V.

Before we can assess whether the VDDA and VREFP can exceed the VDD/VBAT_PMU/VBAT_DCDC supply voltages, the voltage applied to any IO can not exceed (VDD + 0.5V) as specified by limiting values (DS Table 11). So in theory, the analog voltage shall not exceed 2.3V when VDD is powered using 1.8V supply, no matter whether the ADC part and VREF is powered by 3.3V. Please refer to the pad structure described in the UM11126, figure 49 for ESD clamping diode connections on the IO pad.

Another issue while powering the device with 1.8V: Please note that 1.8V is the absolute minimum voltage for device to functional normally, so powering the device with an 1.8V regulator may exceed the operational range of the device, either transiently or constantly.

 

Also, there's a note in the pin description which requires VDDA tied to VBAT_PMU/VBAT_DCDC, so the customer's setup is a direct violation of the following requirement described in DS table 3, and since VREFP's maximum voltage is VDDA, so it's not possible using 1.8V to power the VBAT_PMU/VBAT_DCDC/VDD while using 3.3V to power the VDDA and VREFP:

xiangjun_rong_0-1708499801188.png

 

In general, we do not recommend powering the VDDA using a separate power rail on LPC55S69.

"

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
2 Replies
842 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I will confirm with AE team if it is okay that VDDA is greater than VDD and VBAT_DCDC.

BR

XiangJun Rong

0 Kudos
Reply
818 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I get reply, it is not allowed and VDDA and VREFP are connected to 3.3V, while the digital power supply VBAT_DCDC, VBAT_PMU and VDD are connected to 1.8V for LPC55xx.

 

This is AE reply:

"

I'm assuming customer wants to use 3.3V VREFP and VDDA for measuring analog voltages greater than 1.8V.

Before we can assess whether the VDDA and VREFP can exceed the VDD/VBAT_PMU/VBAT_DCDC supply voltages, the voltage applied to any IO can not exceed (VDD + 0.5V) as specified by limiting values (DS Table 11). So in theory, the analog voltage shall not exceed 2.3V when VDD is powered using 1.8V supply, no matter whether the ADC part and VREF is powered by 3.3V. Please refer to the pad structure described in the UM11126, figure 49 for ESD clamping diode connections on the IO pad.

Another issue while powering the device with 1.8V: Please note that 1.8V is the absolute minimum voltage for device to functional normally, so powering the device with an 1.8V regulator may exceed the operational range of the device, either transiently or constantly.

 

Also, there's a note in the pin description which requires VDDA tied to VBAT_PMU/VBAT_DCDC, so the customer's setup is a direct violation of the following requirement described in DS table 3, and since VREFP's maximum voltage is VDDA, so it's not possible using 1.8V to power the VBAT_PMU/VBAT_DCDC/VDD while using 3.3V to power the VDDA and VREFP:

xiangjun_rong_0-1708499801188.png

 

In general, we do not recommend powering the VDDA using a separate power rail on LPC55S69.

"

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply