LPC55s36 Secondary Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s36 Secondary Bootloader

2,879 Views
henninjw1
Contributor I

Hello,

I am having issues following AN13497.  I am trying to load the bootloader onto the LPC55s36-EVK however the code provided at AN13497SW\boards\lpcxpresso55s36\dual_sbl\lpc55xx_dsbl appears to not be a complete project that I can open/build/flash in MCUXpresso ide. Is the intent to be able to open this project in MCUXpresso ide as I can with following AN12327 for the LPC55s69? What is the best way to build and flash the bootloader given the code provided in AN13497? Thanks

0 Kudos
Reply
3 Replies

2,616 Views
Fredito
Contributor I

HI , I know this has been already discussed, but this is related. I am using the LPC5536 and I did my own bootloader and application. I have problems to jump to the application. I used the jump to application function from  AN13497. Also, the User application startup file for the header is difficult to modify using MCU Expresso. Can you help me on how to set the application header suing MCU expresso?  

0 Kudos
Reply

2,869 Views
dereksnell
NXP Employee
NXP Employee

BTW @henninjw1 ,

Looking at the SBL example included with AN13497, I see the provided example is for ARM's MDK IDE (formerly Keil). The ZIP does not include a project for MCUXpresso IDE.  Perhaps the support engineers here will have more guidance on how to use this example with MCUXpresso IDE.

Best regards

0 Kudos
Reply

2,862 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

I have asked the author of an13497, currently there is only Keil version for the software package as Derek said. Sorry for the inconvenience.

BR

XiangJun Rong

0 Kudos
Reply