LPC55XX ADC Convertion Time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55XX ADC Convertion Time

6,275件の閲覧回数
ray_deng1
Contributor III

Dears,

  As we known, LPC55XX ADC sample ratw is 2MHz, can I know the ADC convertion time?

Thanks & BRs,

Ray

ラベル(1)
タグ(2)
0 件の賞賛
返信
9 返答(返信)

6,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

HI Ray,

This data are not documented.

Please let me know

- Your chip part number?

- what application do you work with LPC55?

Thanks,

Jun Zhang

0 件の賞賛
返信

6,098件の閲覧回数
ray_deng1
Contributor III

Hi Jennie,

   Thanks for your help, 

   The P/N is LPC5512JBD100

    It is used for Environment Detecting Device, which require 16-bit ADC.

Thanks & BRs,

Ray

0 件の賞賛
返信

6,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi 

ADC conversion time should include  sample time and actual conversion time. 

please refer below table,

sampling time is tsampling. conversion time is conversion cycles * ADC clock period

pastedImage_1.png

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

6,098件の閲覧回数
francisy
Contributor II

Hi Jun Zhang, 

According to your table, does LPC5528 support 48MHz adc clock frequency?

BR,

Francis

0 件の賞賛
返信

6,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Francis,

24MHz is for LPC55S2x/6x,  the ADC sample rate is 1Msps.

48MHz is for LPC55S1x,       the ADC sample rate is 2Msps.

Best Regards

Jun Zhang

0 件の賞賛
返信

6,098件の閲覧回数
arimendes
Contributor III

Hi Jun Zhang,

  I would like to know if tsampling can be 62.5nS even for 16-bit resolution.

 Thanks,

 Ari

0 件の賞賛
返信

6,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

yes

0 件の賞賛
返信

6,098件の閲覧回数
ray_deng1
Contributor III

Hi Jennie,

   Got it with many thanks,

0 件の賞賛
返信

6,098件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信