LPC55S6x - LPC55S66JBD100K

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC55S6x - LPC55S66JBD100K

1,627件の閲覧回数
hemalatha_r
Contributor I

Hi NXP team,

As per datasheet page 37 VDD_PMU is tied to FB pin when using internal DC DC Conveter do we have to connect capacitors to it ? Like in EVK LPCXpresso55S69 ?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,515件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi, 

Yes, the capacitor is needed because the DCDC requires at least one cap to have enough power feedback.


Have a great day,
Sol

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,515件の閲覧回数
cmkessell
Contributor I

Is there any further guidance as to how to use the LPC55S69's DC-DC converter (aside from just copying the EVK design) and the recommended component values to attach to the VDD_PMU, FB and LX pins?  The data sheet and user manual don't reveal much.

For example the EVK design has 4 decoupling capacitors attached to the FB-to-VDD_PMU connection - are they all necessary?

0 件の賞賛
返信